Serial devices on a Netbots connected to the same port as a camera pod can cause bot to reboot.
Issue:
Serial devices on a Netbots connected to the same port as a camera pod can cause bot to reboot.
Product Line:
NetBotz
Environment:
All versions
Cause:
RS232-based Serial Devices connected to a USB-to-Serial Port adapter and
USB modems should not share the same USB port or hub as a Camera Pod 120, Camera Pod 160, or a CCTV Pod 120. Doing so may cause configured USB-based Serial devices to disappear and then reappear, or your appliance may unexpectedly restart
Resolution:
Make sure these devices use different ports or hubs.