Technical FAQs

Ask a Question

Maximum warranty period to be covered with NetBotz products

Issue:

Maximum warranty period to be covered with NetBotz products

Product Line:

NetBotz

Environment:

NetBotz warranty

Cause:

Warranty limits.

Resolution:

The maximum time that can be covered under warranty is 5 years. In addition to the standard 2 year hardware warranty on Netbotz products, for both version 2 and version 3 appliances, a maximum of three additional one year extended warranty renewals can be bought for each unit. This gives a maximum coverage of 5 years after the purchase of the product.
 
Was this helpful?
What can we do to improve the information ?