Technical FAQs
Technical FAQs
The IPMI interface is NOT configured by default on NetBotz Central Enterprise. To enable and configure IPMI administrators must use the "IPMI Server Management Configuration Utility". To access this utility a keyboard and monitor must be attached to the NetBotz Central Enterprise system. While the system is booting, press "Control + E" to enter the "IPMI Server Configuration Utility". In some newer systems, this may be listed as BMC.
The following settings should be configured: