Technical FAQs

Ask a Question

Do the VED kits fit onto the roofs of the Symmetra UPS?

Issue:
A customer may want to add a VED Kit to a Symmetra UPS.  

Product Line:
Network Air and Symmetra

Environment: 
All versions and serial ranges.

Cause:
A customer may want to provide cooling to a Symmetra that's installed in a row of cabinets by utilizing Vertical Exhaust Duct Kits.  

Resolution:
The VED kits are not compatible with the Symmetra roof design. 
Was this helpful?
What can we do to improve the information ?