Technical FAQs

Ask a Question

Are the NetShelter CX and CX Mini delivered fully assembled?

Need to know if the NetShelter CX and Mini arrive assembled.

Product Line:
NetShelter CX
All versions and serial ranges.
Customers may ask if assembly is required.
The NetShelter CX Mini arrives on its castors with the brush strip attached to the underside, on a pallet, and the keys inside.
The NetShelter CX arrives on a pallet with ramps supplied. The PDU power cord, leveling feet, keys and documentation are packed separately inside the cabinet.
Was this helpful?
What can we do to improve the information ?