Technical FAQs

Ask a Question

Temperature/Humidity Sensor Duplicate CAN Address. How to address a AP9520TH sensor

 

 

Issue:  
Temperature/Humidity Sensor Duplicate CAN Address 

Product line: 
ACDA901 

Environment: 
All Serial Numbers   

Cause:  
Two or more AP9520TH sensors have the same CAN address 

Resolution:  
This alarm occurs if you have sensors on the a-link chain with the same id address. Please see chart below on how to set the ID a-link address. . 


Was this helpful?
What can we do to improve the information ?