Technical FAQs

Ask a Question

General functions of a MicroAC control platform

Issue:
General functions of a MicroAC control platform
 
Product line:
Airflow
 
Environment:
Data Center Cooling
 
Cause:
 
Resolution:
The MicroAC is an electronic control for the complete management of precision air-conditioners, both in direct expansion versions (with 1 or 2 compressors), with 1 or 2 heating elements or with batteries (valve on the heating battery and/or valve on the cooling battery). The control also allows the management of a humidifier (with CDA type control or Humicontrol) and dehumidification with various pre-settable configurations. In addition, it can also be used in precision units for "Shelters" with management of the condenser fan.
Was this helpful?
What can we do to improve the information ?