Issue: PowerChute Business Edition v9.5 Upgrade Paths
Product: PowerChute Business Edition v9.5
Environment: All supported operating systems
Resolution:
The below table highlights the supported upgrade paths for PowerChute Business Edition v9.5.
Type A UPS
Type B UPS
9.1.1 to 9.5
9.0.3 to 9.5
9.2.0 to 9.5
9.0.4 to 9.5
9.2.1 to 9.5
Type A UPS: Smart-UPS models with prefix SMT, SMX, SURTD and SRT, including models SRC2KUXI, SRC3KUXI, and SRC3KUXIX709. Type B UPS: Smart-UPS excluding UPS models with prefix SMT, SMX, SURTD, SRT.