Technical FAQs

Ask a Question

Why is the NBES0201 Particle Sensor not visible in NetBotz Advanced View

After connecting the NBES0201 Particle Sensor to one of the 4 ports on the NBPD0122 Sensor Pod 120, it is not seen in the list of available sensors in Advanced View.

Environment
NetBotz v2 and v3

Cause
Configuration of External Ports required

Resolution
Go to Configuration in Advanced View.
Under Pod/Sensor Settings, double click on the Sensor Pods icon and then click on the External ports button.
On the Port ID that the particle sensor is connected to, select Particle Sensor PS-100 from the Sensor Type drop-down list.
Assign a Port Label to the sensor if required, and then click OK.
 
Was this helpful?
What can we do to improve the information ?