JAMAICA - Choose Country or Region
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
Voltage Regulators
Surge Protection Devices
Filters & Harmonic Conditioners
Audio-Video Solutions
AV Power Conditioners with Battery
AV Surge Protectors
AV Power Filters
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
Room Cooling Accessories
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
Room Power Distribution
Cabinet Power Distribution
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
SmartShelter Room
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
Data Center Assessment Services
Install
Installation Services
Operate
Remote Monitoring Services
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
When to replace your battery or UPS
UPS Buying Guide
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
JAMAICA - Choose Country or Region
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
What is the cfm rating of the NetShelter CX with AR4703 installed?
Issue:
Customers want to know the cfm rating of NetShelter CX cabinets with the AR4703 fan booster installed.
Product Line:
NetShelter CX.
Environment:
All versions and serial ranges.
Cause:
Installing the AR4703 increases the cfm of the NetShelter CX cabinet.
Resolution:
18U with 1x AR4703 - 260 CFM
24U with 2x AR4703 - 330 CFM
38U with 3x AR4703 - 340 CFM