After installation of PowerChute Network Shutdown on Windows OS when attempting to view web interface the browser displays Page cannot be displayed.
Issue:
Installation of PowerChute Network Shutdown on Windows OS goes smoothly but when attempting to view web interface the browser displays page cannot be displayed and the service PCNS1 and not available to be started.
Product:
PowerChute Network Shutdown (PCNS) versions 3.0 and 3.0.1
Environment:
Windows OS with Java version 7.0.110.21 and above.
Cause:
Changes to Java 7.0.110.21 and above.
Solution:
Upgrade to PowerChute Network Shutdown 4.x
or
1. After the installation completes open a command prompt
2. CD to C:\Program Files\APC\PowerChute\group1 folder. (This is assuming the installation of PCNS was to the default path / folder.)
3. Run the command pcns.exe -install
4. Run the command net start pcns1