Technical FAQs

Ask a Question

What is meant by ‘flooding’ with Air Conditioners?

Issue:
What is meant by ‘flooding’?

Product line:  
All A/C Units with Compressors.

Environment:   
All Serial Numbers.  

Cause:  
Troubleshooting the cause of flooding.  

Resolution:    
Flooding (also known as ‘flood back’) is the term used to describe the condition when Liquid refrigerant reaches the compressor. This occurs when the amount of liquid fed to the evaporator is more than can be evaporated. There are a number of possible causes of flooding including:
• TXV oversized for the application.
• TXV misadjusted (superheat too low).
• System overcharged with refrigerant.
• Insufficient airflow through evaporator.
• Dirty evaporator.
• Evaporator fans not operating.
• TXV bulb not properly attached.
• Power head of TXV is damaged.
Was this helpful?
What can we do to improve the information ?