Technical FAQs

Ask a Question

Loud noise or squealing coming from legacy Airflow unit.

Loud noise or squealing noise.

Product line:
Airflow, AFX, CCT, CM, TC

All Product models, all serial numbers
Possible fan or motor bearing noise.
Loud noises or squealing coming from unit is usually indicative of a fan issue.
  • Bearings need to be check for proper lubrication
  • Blower wheel and housing need to be checked for alignment
  • Fan belt and motor pulley. Check for worn belt or dirty and grease on the pulley.
Was this helpful?
What can we do to improve the information ?