ISX Central 6.2 release notes incorrectly quotes support for Red Hat Linux 6.
Issue:
ISX Central 6.2 release notes incorrectly quotes support for Red Hat Linux 6
Product Line:
InfraStruxure Central
Environment:
InfraStruxure Central 6.2 release notes
Cause:
TIncorrect documentation.
Resolution:
The release notes for ISX Central 6.2 incorrectly list support for Red Hat Linux version 5 and higher. Red Hat 5 has indeed been tested but Red Hat 6 has not. This will be corrected in the next revision of the release notes with the next Central release..