Technical FAQs
Technical FAQs
Issue:
How to Display firmware identification number on an EcoBreeze Expansion Module
Product line:
ACEC200, ACEC201
Environment:
All serial numbers
Cause:
Install
Resolution:
On switch-on, during the start-up test phase, holding the DOWN button, the project identification is displayed for about 2 seconds. The information regarding the
versions/revisions of the project is displayed in sequence. The procedure is exited automatically at the end of the start-up.