Can I use the Camera pod 160 with Netbotz Version 2 appliances (Netbotz 500 and Netbotz 420 models)
Issue:
Will the NBPD0160 camera pod work with the older version 2 NetBotz appliances?
Product Line:
NetBotz
Environment:
Netbotz version 2
Cause:
NetBotz camera pod NBPD0121 is no longer manufactured.
Resolution:
No, a NBPD0160 NetBotz camera pod must be used with a version 3 NetBotz appliance. However, an version 2 NetBotz camera pod (NBPD0121) can be used with a version 3 NetBotz appliance.