Power Specifications for NetBotz 500
*********************************************
-Wallbotz 500 Power Consumption - Maximum Configuration (all ports occupied by max power peripherals)
-Max Power(Wallbotz 500) : 21 Watts
-Power Supply Inefficiency: 15 Watts
-Total Power Used (from Wall Socket): 36 Watts At 120VAC, ( 36Watts is equivalent to ==> 0.3 Amps )
-Wallbotz 500 Power Consumption - Minimum Configuration (Base Unit + 1 docked Camera Pod + 1 docked Sensor Pod)
-Min Power(Wallbotz 500) : 8 Watts
-Power Supply Inefficiency: 6 Watts
-Total Power Used (from Wall Socket): 14 Watts At 120VAC, 36Watts ==> 0.12 Amps
**NOTE:
-These calculations do not take into account Power Factor for this power supply.
-The power factor may affect how much current is actually used from AC wall outlet.