Technical FAQs
Technical FAQs
Begin Purge | Identify the percentage of total capacity that will initiate a purge. |
End Purge | Identify the percentage of total capacity that will cause the purge to end. |
Warn of Purge | Identify the percentage of total capacity that will result in a warning that a purge may occur soon. |
Send Warning E-mails | Select to send e-mails to the StruxureWare Data Center Expert Administrators that include an e-mail address as part of their user credentials, when the Warn of Purge threshold is reached. |
Apply Purge Settings | Click to save changes to the settings. |
Purge Data Created On or Before | Select the date for which all data stored on or before that date will be purged. |
Choose the Types of Data to Manually Purge | Select to include Alarm History Data, Alarm Binary Data, Sensor Data, Untagged or All Surveillance Data, or a combination of these choices, in the manual purge.Note: You can prevent tagged surveillance data from being purged by selecting Untagged Surveillance Data instead of All Surveillance Data. |
Run Manual Purge | Click to purge the selected data for the defined range of dates. |