Technical FAQs

Ask a Question

How to Brain Dead a Back-UPS unit. (Purge charge in units "brain" to reset)

Issue:

To brain dead a Back-ups is to purge the charge in the brain of the UPS.

Product Line:

Back-UPS, Back-UPS Pro

Environment:

N/A

Cause:

Troubleshooting procedure.

Resolution:

To do this, follow the below procedure;
 

1: Disconnect any attached load.

2: Unplug the UPS from the wall socket.

3: Disconnect the UPS' internal battery.

4: Push and hold the ""On"" button on the UPS for 5 seconds

5: Reconnect internal battery.

6: Plug UPS in to known good power source.

7: Turn UPS on.


 
Was this helpful?
What can we do to improve the information ?