IRAQ - Choose Country or Region
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
Voltage Regulators
Surge Protection Devices
Filters & Harmonic Conditioners
Mobile Accessories
Portable Device Chargers
Cooling
Cooling
Cooling
Modular Access Floor
Uniflair Technical Floor
Uniflair Office Floor
Uniflair Building Floor
Air Economizers
Ecoflair Air Economizers
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
Static Transfer Switches
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
Module Optimized Cooling
Chilled Water System
Power Modules
Enclosed Power Module
Skid Mounted Power Module
IT Modules
SmartShelter Container
SmartShelter Module
SmartShelter Data Hall
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
Data Center Assessment Services
Install
Installation Services
Operate
Battery Replacement Services
Extended Warranties
Preventive Maintenance
Service Plans
Optimize
Training Services
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
IRAQ - Choose Country or Region
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
Version 1 Appliance Will Not POST to NetBotz Central 2.x
Issue:
Version 1 Appliance Will Not POST to NetBotz Central 2.x
Product Line:
NetBotz
NetBotz Central
Environment:
NetBotz version 1
NetBotz Central 2.x
Cause:
Troubleshooting posting issues.
Resolution:
First, browse to the bot in question and check the PICPOSTURL field:
http://ip-of-wallbotz/http.txt
If the \""PICPOSTURL\"" doesn't have the port specified, it's the standard port 80, otherwise it should be whatever follows the hostname of the NBC.
If you want to change the port or the hostname/IP of the NBC, you’ll type the following in the URL field of the bot:
http://ip-of-wallbotz/setHttp?PICPOSTURL=http://ip-or-hostname-of-nbc-server:PORT/central/photoman
Note: If the ports are correct, and the hostname is correct, make sure the appliance can resolve the hostname of the NBC. To do this, telnet to the appliance and do a \""gethostbyname nbc-server-name\"".