Technical FAQs

Ask a Question

Lets Learn How to set the sensitivity for BE800-IND ?

Please follow the below steps :

Important Note:
> Ensure that the Back-UPS is Off but  connected to utility power.
> Ensure that the Load's are not connected with the Back-UPS.


Step 1 :Press the front panel pushbutton fully inward for 10 seconds. All indicators
on the Back-UPS will flash to acknowledge going into Programming Mode ,The Back-UPS will then indicate its current Sensitivity Setting


To select the Low Sensitivity setting, press the pushbutton until indicator flashes "Green"

To select the Medium Sensitivity setting, press the pushbutton until indicator flashes "Amber"
To select the High Sensitivity setting, press the pushbutton until indicator flashes "Red"

To exit without changing the Sensitivity Setting, press the pushbutton until the green indicator is flashing.
Once in Programming Mode, if the pushbutton is not pressed within 5 seconds, the Back-UPS will exit Programming Mode; all indicators will extinguish.

To understand easily , watch the video below 




Was this helpful?
What can we do to improve the information ?