Technical FAQs

Ask a Question

What is the function of Load Indicator LED in PDU AP7921B ?

The load indicator LED identifies near-overload (warning) and overload (critical) conditions for the Rack PDU.                                                                                                                                
Solid Green--OK. No near-overload (warning) or overload (critical) alarms are present.                                                                                                                                                                                          
Solid Yellow--Warning. At least one near-overload (warning) alarm is present, but no overload (critical) alarms are present.                                                                                                 
Flashing Red-- Overload. At least one overload (critical) alarm is present.

 
Was this helpful?
What can we do to improve the information ?