Technical FAQs

Ask a Question

What is new release in Powerchute Business Edition 9.2V ?

The following features are new to PowerChute Business Edition v9.2:
• New SMTP Port option in PowerChute Email Settings screen.
A new option has been added to the PowerChute user interface to specify the SMTP port from which mail
is sent.
• Security enhancement - fix for POODLE: SSLv3 vulnerability (CVE-2014-3566).
JRE 1.8u31 is now bundled with PowerChute Business Edition v9.2. SSLv3 is disabled by default.
Note: SNMP is enabled by default. It can be disabled in SNMP Settings on the Web Agent, or for certain
Agents, it can be disabled in the Console.
Was this helpful?
What can we do to improve the information ?