Technical FAQs

Ask a Question

Video: How to disable Battery Saver Mode for BX600CI-IN ?

To disable battery saver option,kindly follow the below steps :

* Press the BATTERY SAVER button to deactivate the battery saver feature.

* Battery saver LED will turn off indicating that the battery saver mode is disabled .

Note:  If the load is less than 40 watts we would sugget to disable battery saver mode.We recommend the battery saver mode to be enabled if the load is more than 40 watts for the enchancement of battery life.

Was this helpful?
What can we do to improve the information ?