Technical FAQs

Ask a Question

Video: How to enable Battery Saver mode in BX600CI-IN ?

To enable battery saver option, kindly follow the below steps :

* Press the BATTERY SAVER button to activate the battery saver feature.

* Battery saver LED will illuminate to indicate the UPS is working in the battery saver mode.

* This feature helps the UPS to enhance the battery life . Runtime of the connected equipment will reduce when this feature is enabled.

  Note: Minimum of 40 watts of load should be connected when battery saver option is enabled .

Was this helpful?
What can we do to improve the information ?