Technical FAQs

Ask a Question

Video: How to set the sensitivity setting for BE650Y-IN ?

To set the sensitivity settings kindly follow the below steps :
1. Connect the Back-UPS to a utility power source. The Back-UPS will be in Standby mode. No LED will be illuminated.
2. Press and hold the POWER ON/OFF button until the LED flashes alternately green-red-amber. Release the button. The Back-UPS is now in Program mode.
3. The Power On LED will flash either green, amber, or red to indicate the voltage sensitivity level. Re
4. To select LOW sensitivity, press the POWER ON/OFF button until the LED flashes green.
5. To select MEDIUM sensitivity, press the POWER ON/OFF button until the LED flashes amber.
6. To select HIGH sensitivity, press the POWER ON/OFF button until the LED flashes red.
7. To exit Program mode wait five seconds and all LED indicators will extinguish. Program mode is no longer active.

 
Was this helpful?
What can we do to improve the information ?