Technical FAQs

Ask a Question

Cannot access the command line interface remotely of NMC card AP9635 ?

Possible cause & Solution:                                                                                                                                                                                                                                                                                                                
• Make sure you are using the correct access method, Telnet or Secure SHell (SSH). An Administrator can enable these access methods.
By default, Telnet is enabled. Enabling SSH automatically disables Telnet.                                                                                                                                                                                                                                                                                                                                                 
• For SSH, the NMC may be creating a host key. The NMC can take up to one minute to create the host key, and SSH is inaccessible for that time.

Was this helpful?
What can we do to improve the information ?