Technical FAQs

Ask a Question

What to do if SURT6000XLI-CC is Not powering on?

Follow the below steps for the solution :

1.Check that the battery connectors are fully engaged.
2.Press the test button once to power the UPS and the connected equipment.
3.Check that the power cable from the UPS to the utility power supply is securely connected at both ends 4.Check the utility power supply to the UPS by plugging in a table lamp. If the light is very dim, have the utility voltage checked. 
Was this helpful?
What can we do to improve the information ?