Technical FAQs

Ask a Question

How do we Install a mini-GBIC (SFP) transceiver in AP9224112 ?

Follow the below steps : To install a mini-GBIC (SFP) transceiver:

1. Insert the transceiver into the mini-GBIC port with the exposed section of PCB board facing down.
2. Push the transceiver firmly until it clicks into place.
3. The switch automatically detects the installed transceiver. Check the LEDs to verify that it is functioning properly
Was this helpful?
What can we do to improve the information ?