Technical FAQs

Ask a Question

What type of cable's are used to connect the switch to network in AP9224111 ?

Following Cable's are used to connect the switch to network in AP9224111   :  

> The RJ-45 ports use either unshielded twisted-pair (UTP) or shielded twisted-pair (STP) cable.
Was this helpful?
What can we do to improve the information ?