Technical FAQs

Ask a Question

How to apply power to AP9224112 APC Ethernet Switches?

Follow the below steps to power on AP9224112 APC Ethernet Switches :

>Connect the cord of the power adapter to the power socket on the rear panel of the switch.
>Connect the other end of the power cord to an APC UPS that is connected to a power outlet.
>Check the power indicator on the front panel to make sure that the switch is receiving power.  
After you connect the power cord of an AP9224112, use the power switch on the rear panel to supply power to the unit.
Was this helpful?
What can we do to improve the information ?