Technical FAQs

Ask a Question

It is possible to connect Two SRC3KUXI UPS in parallel connection to achieve redundancy ?

Yes, it is possible to connect two SRC3KUXI ups in parallel by using redundant kit called SRCPK0203.                                                                                                                                                       
Note: Parallel system SRCPK0203 works with only two identical UPS models of SRC2KUXI or SRC3KUXI
Was this helpful?
What can we do to improve the information ?