Technical FAQs

Ask a Question

What is the maximum distance between the Rack LCD (AP5717) Console and the target device (KVM Switch or Server) ?

 The maximum distance between the Rack LCD Console and the target device (a KVM switch or server) is 32.8 feet (10m).
Was this helpful?
What can we do to improve the information ?