Technical FAQs

Ask a Question

How to Install Hardwire PDU (AP7520) with any UPS ?

Follow the below steps : 1. Locate the hardwire terminal block cover on rear panel of UPS. Remove
the screw securing the cover and remove the cover.
2. Remove the knockout from the cover3. Connect the line, ground and neutral wires from the UPS, to the terminal
block through the cover. Terminals are labeled for proper wire
configuration.
4. Replace and secure the cover removed in step 1.
5. Locate the hardwire terminal block cover on rear panel of PDU. Remove
the screw securing the cover and remove the cover.
6. Remove the knockout from the cover.
7. Connect the line, ground and neutral wires to the terminal block through
the cover. Terminals are labeled for proper wire configuration.
8. Replace and secure the cover removed in step 5.
Was this helpful?
What can we do to improve the information ?