Technical FAQs

Ask a Question

"What to do if the circuit breaker on the PDU (AP7520) has tripped ?"

Follow the below steps :Disconnect equipment from the PDU. Reset the circuit
breaker. Reconnect equipment. If the circuit breaker
trips again, disconnect the device that caused the short
circuit
Was this helpful?
What can we do to improve the information ?