Technical FAQs

Ask a Question

What to do if UPS is not turned on connected with AP7520 ?

Follow the below steps : 
Press and hold the POWER ON/OFF button until a short
beep is heard to turn on the UPS.
Was this helpful?
What can we do to improve the information ?