Technical FAQs

Ask a Question

What are the different ranges of input voltage which can be customized in STS60 model ?

Please find the ranges of voltages which can be customized in STS60 model: 380/400/415 V
Was this helpful?
What can we do to improve the information ?