Technical FAQs

Ask a Question

What If the communication card green indicator remains continuously off in STS160 Model ?

Follow the below steps :
◗ Check the card is correctly inserted into its slot and its protective cover is correctly screwed-on.
◗ Check the STS is powered.
◗ Remove the card and re-insert it.
Was this helpful?
What can we do to improve the information ?