Technical FAQs

Ask a Question

How to do Upsilon STS customization for STS400 ?

Follow the below steps : 1 - Press the menu button.
2 - Select "Setup", then "Customization" using the function buttons marked up arrow or down arrow.
3 - Confirm the order by pressing the function button  .
4 - Enter the password.
1 - Press the manual transfer button - 25 :
2 - Enter the password by following the
instructions on the display.
3 - validate the password by pressing the
grey function button  - 23 marked on the
screen.
LEDs  -24 and  - 27 flash.
After the transfer, the green LED - 27 goes
on.
The load is supplied by Source 2
Was this helpful?
What can we do to improve the information ?