Technical FAQs

Ask a Question

How to startup or turn the STS630 on ?

Follow the below steps : 
1 - Check that the two sources are
energised (voltage present).
2 - Set circuit breakers Q4  and Q6 
to the ON position (position 1).
3 - Turn switch Q1BP to the ON position
(position 1). 
The load is supplied by Source 1 via the
bypass.
4 - Set switches Q1 and Q3  to the
ON position (position 1). 
5 - Turn switch Q1BP  back to the OFF
position (position 0). 
6 - Set switch Q2 to the ON position
(position 1). 
The load is supplied by Source 1
Was this helpful?
What can we do to improve the information ?