Technical FAQs

Ask a Question

How to SET USERNAME AND PASSWORD in ADM submenu function for AP5201 model ?

Follow the below steps :

Set usernames and passwords for one Administrator and
four Users:
1. Select either the Administrator or User field.
2. On the User Setup screen, enter a username and a
unique password consisting of up to 15 alphanumeric
3. Re-enter the password in the Confirm field, and press
ENTER. Press ESC to return to the previous menu.
NOTE: To modify or delete an existing username or
password, press BACKSPACE to erase the characters.
CAUTION: For effective security, you must enter usernames
and passwords for four Users and the Administrator. If you
leave any username or password field blank, an
unauthorized user can log on without entering a username
and password.
Was this helpful?
What can we do to improve the information ?