Technical FAQs

Ask a Question

How to Disable the power-saving function in Back-UPS BR1500GUXI ?

Kindly follow the below steps to Disable the power-saving function in Back-UPS BR1500GUXI :
  • Press and hold MUTE and DISPLAY simultaneously for two seconds.
  • The Back-UPS will beep to indicate that the feature is disabled.
  • The leaf icon on the display will disappear.
Was this helpful?
What can we do to improve the information ?