Technical FAQs

Ask a Question

How to Disable the power-saving function in Back-UPS BR1000GUXI ?

Kindly follow the below steps to Disable the power-saving function in Back-UPS BR1000GUXI :

Press and hold MUTE and DISPLAY simultaneously for two seconds, UPS will beep to indicate that the feature is disabled.
The leaf icon on the display will disappear.
Was this helpful?
What can we do to improve the information ?