Technical FAQs

Ask a Question

Can we schedule to disable battery back-up alarms when the PC is in hibernation in PCPE

Yes, Open the application, click on 'Notification' under the 'Confuguration' menu, select 'Disable the battery backup alarms when the PC is in hibernation' and select the timeline.
Was this helpful?
What can we do to improve the information ?