Technical FAQs

Ask a Question

What is the type of Input connector is used in AP9559?

Please find the Input Connector type below: IEC-320-C20
input connector
(16A @ 240 V; 20A @ 120 V) used with detached power cord (supplied).
Was this helpful?
What can we do to improve the information ?