Technical FAQs

Ask a Question

What is the type of Input connector is used in AP9565?

Please find the Input Connector type below : IEC 320 C20 inlet
Was this helpful?
What can we do to improve the information ?