Technical FAQs

Ask a Question

If the LCD display is showing BDC error in SRCE6KUXI model?

· UPS is turned on without connecting the battery system.
· Bad battery is connected i.e voltage is less than 180 V.
· Battery connection might be loose, either from UPS or from battery end.
Was this helpful?
What can we do to improve the information ?