Technical FAQs

Ask a Question

If the LCD display shows fault as SIT in SRCE6KUXI?

If the LCD display shows fault as SIT in SRCE6KUXI. Contact the local electrician and ask the electrician to check for the following condition
  • L-N (Line-Neutral) reversal or missing earth connection. 
  • When potential difference between N & earth is more than 20V.  
  • Get the earth connection checked.
Was this helpful?
What can we do to improve the information ?