Technical FAQs

Ask a Question

What to do if the UPS SRC2KUXI is Toggling between on mains to on battery?

To resolve the issue , kindly follow the below steps 

· Check whether input cord is plugged correctly.
· Check with the input power supply range.
· If still problem persist the problem can be resolved by firmware upgrade.
Was this helpful?
What can we do to improve the information ?