Technical FAQs

Ask a Question

What to do if my UPS(SURT20KUXI) is showing "UPS Is Overloaded"?

Follow the steps, UPS(SURT20KUXI)

Option 1) Decrease the load.
Option 2) Check the load distribution on the three phases through the PowerView display.
If the load is unevenly distributed, adjust the load distribution.
Was this helpful?
What can we do to improve the information ?